Readme: Timer Interrupts in C frameworks example (08/3/00)
----------------------------------------------------------

When this program is run, users will be able to light the seven segment 
LED on the EZ-USB Development Board with a 0-9 count, and control the 
step rate (1s - 5s) using BULK OUT endpoint transfers from the 
EZ-USB Control Panel. This example utilizes frameworks.

Please refer to the application note "EZ-USB Timer interrupts in C" for a complete 
description.


-------------------------------------------------------------------------------
File: 		timer0.c
Contents:	Programmable timer interrupt that controls step interval 
 		(ranging from 1-5 s) of LED display from 0-9, using 
		endpoint control from the Control Panel. 

Length Field: 		Controls how many times the 0-9 count will loop.
Hex Bytes Field: 	Controls how fast the count steps

			1) 01h -> 1s
			2) 02h -> 2s
			3) 03h -> 3s
			4) 04h -> 4s
			5) 05h -> 5s

Copyright (c) 2000 Cypress Semiconductor. All rights reserved
-------------------------------------------------------------------------------
Note: Please place this example under the C:\Cypress\Usb\Examples\Ezusb 
sub-directory